Search

Start main contents

  • Register
  • Login

Solutions

Print page

Solutions

Rotary cutter

Run your Cutter and reduce costs with Mitsubishi Electric

Overview

Rotary knife applications involve 2 axes of servo to continually or intermittently perform a cut, labeling procedure, or stamping process where the servo axis 1 aligns itself to move at the same speed as a feed axis 2 that drives a material to be cut/stamped/labeled. The servo axis 1 (or slave axis) moves according to the feedback of the axis 2 driving the belt (master axis) so that it can coordinate its movement with speed changes.

Which automation components are important

The LD77MS provides a simple solution rotary knife application. With high speed registration capability, Auto-Cam-generation, and electronic pulse compensation functionality during non-cut regions, the LD77MS can accurately respond to input pulses from an external encoder or a servo master axis.

Application

In a typical rotary knife application, the servo motor continually moves. If the distance between cuts is small (smaller than the circumference of the cutter), the motor speed during the non-cut compensation region is faster than the conveyor speed and vice versa. In this type of application, the cut length, label or stamp location may change and it is possible that the feed material may slip, stretch, or bind up, causing the operation’s accuracy to change. The addition of a mark sensor before the servo axis can help to compensate for these fluctuations.


MelPackAL – Solution for your packaging machine – The Mitsubishi Electric solution for your packaging machine - conform with the OMAC PackML and PLCopen standards.
Find out more
Page top