Start main contents

  • Register
  • Login

Solutions

Print page

Solutions

Secure MES

Over the last few years Mitsubishi Electric has been developing technology which challenges the traditional automation architecture and can offer a robust environment whilst delivering the operational requirements needed.

Over the last few years Mitsubishi Electric has been developing technology which challenges the traditional automation architecture and can offer a robust environment whilst delivering the operational requirements needed.

Mitsubishi’s “C Controller” range of automation solutions offers direct connection from the plant/asset to enterprise systems such as SAP, Oracle, DB2 etc within a ruggedized industrial form factor. These systems are non PC based and are therefore not susceptible to the same operating system legacy issues that are found in a traditional PC based system.

In addition, Mitsubishi has developed intelligent solutions to provide data and alarm logging to be carried out locally at the PLC. This technology has created the possibility of removing the gateway PC from the topology altogether.

By using the Mitsubishi C Controller technology the link between plant/asset and the enterprise can be achieved directly from the PLC level and therefore minimising the risk.

In a world where information and data security is becoming ever more important the MES IT module allows user access to be tailored to their information needs. IT teams can access automation process data without fear of inadvertently affecting operational processes while still allowing engineering staff to carry out their normal functions with no risk to IT infrastructures.

Page top