• Register
  • Login

Products

Print page

MAPS

Reducing your engineering effort and cost

Mitsubishi Electric and e-F@ctory partner Adroit Technologies have addressed the shortcomings of traditional PLC-SCADA integration tools with Mitsubishi Adroit Process Suite (MAPS).

The Product

The Mitsubishi Adroit Process Suite (MAPS) is a life-cycle software tool that offers value along the entire value chain. It addresses the shortcomings of most PLC SCADA integration tools in that it offers value to the engineering and integration phases. It also extends the integrity of the “as delivered” solution and offers customers the ability to handle the normal extensions and maintenance of any automation solution.

Wizard approach

MAPS provides a wizard approach which can automatically generate PLC and SCADA projects, significantly reducing the time spent on development and configuration. It also ensures a standardised and structured design which eases on-going maintenance of the plant throughout its life-cycle.

Reporting

With MAPS, reports covering areas such as I/O schedules, PLC and SCADA tag configuration can be automatically generated. This automatic report generation ensures that the project on handover also reflects the “as built” up-to-date electrical and instrumentation drawings that are aligned to the SCADA tags and PLC I/O. The reports are database driven, so even through on-going maintenance the reports will always reflect the current status of the electrical and instrumentation configuration.

Benefits

  • Standards approach to projects
  • Single point of configuration, deployment and management
  • Automatically generated PLC and SCADA projects to reduce engineering effort
  • Automatically generated reports
  • On-going life cycle management

Documentation

MAPS also helps to ensure that project documentation is kept up to date. Throughout the design phases and even as systems are upgraded or modified over time, MAPS provides on-going management of the PLC/SCADA and the plant “as built” electrical and instrumentation documentation.