• Register
  • Login

News Center

Print page

Software

Get your original sources

Latest News

2019-01-08 – New benchmark SCADA software platform

MAPS 4, the latest SCADA solution from Mitsubishi Electric for control and visualisation, extends connectivity options, adds user tools and increases the scope of its built-in functionality. The result is a software suite that can reduce the time taken for project development and integration, while also enabling users to realise Smart Factory objectives.

Software

2018-11-28 – How to achieve faster SCADA projects

Within the myriad of possible applications for SCADA software there is a common theme for both the end user and system integrator, and that is a need to respond to competitive pressures. The reason manufacturing, process, logistics and utility businesses all invest in new control and monitoring software is to build more efficient, cost-effective operations.

2018-11-28 – Holistic Solutions for Smart Manufacturing

As digitalization, Big Data and the Industrial Internet of Things (IIoT) take their course, the classical linear manufacturing model is changing: Complex, integrated networks are developing that aim to achieve higher productivity with lower resource consumption. Machines, devices and applications must become smarter accordingly. When it comes to investment decisions, cooperation with ...

2018-05-17 – Effective control of water distribution networks and processing facilities

IFAT 2018, 14th –18th May 2018, Munich, Hall C1 / Stand 440 Since incomes for operating companies and government authorities in the water industry are either fixed or hard to change, reducing costs is a strong driving force behind any investment. At the IFAT exhibition 2018, Mitsubishi Electric is presenting its life-cycle management solutions that can support overall efficiency by reducing ...

2018-05-16 – Optimised municipal water management by artificial intelligence

Process management, visualisation and control package Aquatoria® is delivering balanced water pressure across urban distribution networks, significantly improving water service levels, reducing leaks and lowering energy usage. The ideal situation for any water utility operator is to provide a service as close to perfect as possible.

2018-03-22 – Preview IFAT 2018 - Solutions for improving operations and reducing costs

As the water industry drives for increased efficiency in every area, completely integrated solutions that offer improvements to operational insight, energy usage, physical supply networks and process installations are of high importance. At the IFAT 2018 exhibition, Mitsubishi Electric will be presenting its approach to meeting these needs, which has been developed based on an understanding of ...

2018-02-27 – Faster time to market

Consistent data exchange between electrical wiring and control software through AutomationML Mitsubishi Electric has implemented the AutomationML interface within iQ Works, the integrated software suite for programming Mitsubishi Electric automation products. AutomationML represents an important step-change in the way complex equipment is designed ...

2017-05-04 – Innovative solutions for Packaging machines support industry 4.0 drivers

Easier machine integration via PackML and programming using S/W function blocks are key themes. Today’s packaged goods manufacturers face challenges to reduce costs per package unit - using production lines that also need to be flexible and ready to accommodate new packaging machine solutions. At the same time, production lines...

2017-04-12 – Mitsubishi Electric launches the ‘Industrial Internet of Industrial Sewing Machines’

Visitors of the Texprocess can see how Industrial Internet of Things (IIoT) connectivity boosts productivity and increases quality for users of Mitsubishi Electric industrial sewing machines in the context of Industry 4.0.

2016-06-16 – Preview PowerGen - Building a predictable future for power generation

The power generation industry is facing up to increasingly demanding challenges, driven by requirements for increased flexibility, greater efficiency and improved predictability. At POWER-GEN Europe, Mitsubishi Electric will be showing visitors how its proven, safe and reliable solutions can address these key themes in the energy market.

2016-06-09 – Where Virtual meets Reality - creating and operating a Virtual Power Plant

The amount of electricity produced using renewable energy sources is subject to fluctuations, making the network unstable. Conventional power plants can be used to balance out the situation. However, the problem with these is their negative CO2 balance and lack of flexibility. Virtual power plants can ensure stability by automatically combining renewable energy sources based on availability.

2016-06-07 – PMSX®pro Web Monitoring – Plant control at a glance

ME-Automation Projects GmbH, a sister company of Mitsubishi Electric, has introduced a new functionality called “PMSX®pro Web Monitoring” to expand the proven, future-oriented process control system PMSX®pro.

2016-06-01 – Preparing the water industry for the future: identifying and implementing trends

In order to remain fit for the future, water supply and distribution facilities need to set themselves special challenges and take future trends seriously. Topics such as system migration and modernisation, data capture and analysis or preventive maintenance are becoming increasingly important when it comes to ensuring a high level of plant availability and efficient operation.

2016-04-21 – Preview IFAT - Making optimum use of sewage, waste and renewable resources

Mitsubishi Electric will be presenting its comprehensive engineering expertise as a provider of complete solutions for water, sewage, waste and raw materials management at IFAT 2016 (Hall A5.243). Numerous successfully implemented turnkey and customised EI&C projects, such as water/sewage systems as well as solutions for producing energy from waste, biomass or biogas will be demonstrated.

2016-03-22 – Preparing pharmaceutical and medical technology for the future

Production environment requirements in the pharmaceutical and medical technology sectors are very high. Not least, the strict cleanroom criteria present a particular challenge. In order to survive in a highly competitive market, companies also need to make sure that they increase their production effectiveness and minimise costs. Current trends include process optimisation for the purpose of ...

2016-03-15 – Mitsubishi Electric integrates own Factory Automation products to optimise building management processes

The Factory Automation Division of Mitsubishi Electric Europe B.V. has installed an extensive range of building automation and security products in the newly built German Branch in Ratingen. The products and solutions can be used for a variety of applications, for example quantifying, measuring, displaying, recording and monitoring current and voltage flows around the building. All the data ...

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2015-09-17 – Mapping the clearest route to project completion

RWM exhibition, Birmingham, 15.-17.9.2015 Whether it is for a small renewable energy plant or a full-scale power station, often the hardest part of a control engineering project is the start. A popular and market-proven tool from Mitsubishi Electric and its e-F@ctory partner Adroit Technologies not only makes the planning stage easier, but also helps reduce the time and cost to completion of...

2015-09-17 – New hybrid power source (HPS) energy management system can select best source while also reducing consumption by up to 30%

RWM exhibition, Birmingham, 15.-17.9.2015 Reducing energy consumption is just one part of an industrial company’s energy management strategy, it must also source or generate its energy competitively, while taking account of CSI and green initiatives which may affect the energy mix. This situation opens up the requirement for a solution that can make complex purchasing and management decisions..

2015-09-17 – Make renewable and EFW plants more efficient with the global experience of Mitsubishi Electric

RWM exhibition, Birmingham, 15.-17.9.2015 Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure the maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-08-13 – Virtual power plants - A reliable source of energy for the future

The amount of electricity produced using renewable energy sources is subject to fluctuations, making the network unstable. Conventional power plants can be used to balance out the situation. However, the problem with these is their negative CO2 balance and lack of flexibility. Virtual power plants can ensure stability by automatically combining renewable energy sources based on availability.

2015-06-30 – Mitsubishi Electric Europe shows how to get the most from waste to energy and renewable resources

Mitsubishi Electric has a proven track record of supplying turnkey Electrical, Instrumentation and Control (EI&C) projects for energy producers including full engineering and commissioning. This includes systems for Energy from Waste, Biomass and related industries, such as Biogas based generation for Waste Water clients – covering both electricity generation from steam turbines and district ...

2015-04-14 – Reduce your engineering costs by up to 50% with Mitsubishi Adroit Process Suite (MAPS) and Eplan Electric P8

At SPS IPC Drives 2014, Mitsubishi Electric demonstrated the integration of the Mitsubishi Adroit Process Suite (MAPS) with Eplan Electric P8 data for the first time, underlining the positioning of MAPS as an integrated automation lifecycle software solution. The integration enables Eplan Electric P8 users to generate a MAPS project directly from Eplan Electric P8 circuit diagrams.

2015-04-02 – Preview - Solutions for the water industry at the "PUMPENplatz"

Mitsubishi Electric will be presenting an innovative portfolio of solutions designed specially for the water industry at the "PUMPENplatz" at Hanover trade fair on Stand G43, Hall 15. Providing consumers with clean drinking water is a vital process but handling waste water correctly is also an extremely critical issue. Strict requirements such as the Urban Waste Water Treatment Directive provide..

2015-02-10 – Integrated solutions reduce life-cycle costs in the water sector

As an exhibitor on the joint stand of German Water Partnership e.V. at this year's Wasser Berlin International to be held from 24 to 27 March, Mitsubishi Electric will be focussing on cost-effective life-cycle management in the water sector. The automation experts will be providing visitors with information on the topics of energy management, condition monitoring and preventive maintenance...

2015-02-05 – Coordinating virtual power plants intelligently

At this year's trade press days, Mitsubishi Electric focussed on renewable energies. In his expert presentation entitled "Virtual power plants–a reliable source of energy for the future", Dag Hoeft, Process Industry Technical Sales Consultant, Mitsubishi Electric Europe B.V., looks at backgrounds and trends in renewable energies, explains the significance of virtual power plants for the energy...

2014-11-28 – MAPS HMI - Mitsubishi Electric offers a cost efficient solution for SCADA control

Mitsubishi Electric has developed a new cost-efficient software, named “MAPS HMI” (Mitsubishi Adroit Process Suite – Human Machine Interface) based on the highly successful MAPS software. The new software is a lite version with reduced functionality which will be particularly attractive for applications with simpler HMI requirements, which do not need the capabilities of a full SCADA solution.

2014-11-11 – Regenerative energy, reduction of energy peaks and innovative products – the highlights at SPS IPC Drives

Visitors to the Mitsubishi Electric stand 380 in hall 7 at this year's SPS IPC Drives can expect to see a range of innovative factory automation products based on Industry 4.0. The highlights will include the Energy Assist Unit, the MR-J4-TM servo controller and the new GS series HMIs.

2014-09-29 – Energy from Waste sector gets ready for expansion and development

Mitsubishi Electric’s first-time presence in the EfW (Energy from Waste) hall at the Resource Efficiency and Waste Management show (RWM) in Birmingham, UK, has been hailed as an immediate success.

2014-09-02 – MAPS HMI - Mitsubishi Electric offers a cost efficient solution for SCADA control

Mitsubishi Electric has developed a new cost-efficient software, named “MAPS HMI” (Mitsubishi Adroit Process Suite – Human Machine Interface) based on the highly successful MAPS software. The new software is a lite version with reduced functionality. It will be particularly attractive for applications with simpler HMI requirements, which do not need the capabilities of a full SCADA solution.

2014-08-05 – Mitsubishi Electric demonstrates world class capabilities in energy from waste

Mitsubishi Electric Europe will be exhibiting at RWM 2014 – the resource efficiency and waste management show, being held in the National Exhibition Centre, Birmingham UK, 16-18 September 2014. For more than 25 years Mitsubishi Electric has been one of the leading suppliers for the Energy from Waste (EfW) industry. It will be displaying its solutions on stand 4C44-D45 in hall 4 & 5 ...

2014-02-06 – Making bakery production future-ready thanks to data transparency

At this year’s trade press days in Karlsruhe, Mitsubishi Electric is switching the focus to the bakery industry with its presentation “Increasing Productivity through Automation Technology in the Food Industry”. Stefan Knauf, Corporate Account Manager Food & Beverage, CPG, at Mitsubishi Electric’s Factory Automation – European Business Group, will look at options for improving efficiency...

2014-01-28 – e-F@ctory Alliance welcome Eplan as new member

In parallel with Eplan joining the e-F@ctory Alliance, Mitsubishi Electric Europe have been welcomed into Eplan’s “Community of efficient engineering”. This was agreed between Maximilian Brandl, Chairman of Eplan’s board of Management, and Hartmut Pütz, President of Mitsubishi Electric’s European Factory Automation Business Group, during a meeting at the SPS IPC Drives fair 2013 in Nuremberg...

2014-01-07 – Mitsubishi Electric launches its high performance HMI/SCADA software, MAPS, in Scandinavia

Mitsubishi Electric has launched MAPS (Mitsubishi Adroit Process Suite) in the strategically important regions of Scandinavia and the Baltic States. Mitsubishi explains that MAPS offers much more than a simple SCADA system. It is a complete life-cycle management tool. One of its main benefits is almost infinite scalability: MAPS can be used for complex process-oriented solutions...

2013-11-26 – Mitsubishi Adroit Process Suite 3.0 perfects life cycle management

Mitsubishi Electric will be presenting the next generation, version 3.0, of MAPS (Mitsubishi Adroit Process Suite) at this year’s SPS IPC Drives (Hall 7, Stand 380). MAPS 3.0 is the optimised HMI/SCADA life cycle management software that offers virtually unlimited scalability for versatile use.

2013-12-12 – Mitsubishi provided a look at its future automation solutions at SPS IPC Drives 2013

At this year's SPS IPC Drives, Mitsubishi Electric provided visitors with a look into the future of its automation solutions. For the first time in Europe, the successors to the globally popular compact MELSEC FX PLC series and the latest generation modular MELSEC iQ Platform were on show, alongside the new GOT2000 series touch screen HMI and the new FR-A800 high-end frequency inverter range.

2013-11-21 – AUVESY joins Mitsubishi Electric’s e‑F@ctory Alliance

Company AUVESY GmbH & Co KG has joined the e‑F@ctory Alliance, a partner initiative of Mitsubishi Electric Europe for offering market leading industrial automation solutions. The German company AUVESY, located in Landau, are experts in automated backup and version control of software used in manufacturing and production environments.

2013-11-11 – Next Generations – Experience the future live at SPS IPC Drives

At this year's SPS IPC Drives, Mitsubishi Electric will be giving visitors a closer look into the future of its automation solutions. For the first time in Europe, the successors to the compact MELSEC FX PLC series and the modular automation concept MELSEC iQ Platform, the brilliant HMI GOT2000 series and the FR-A800 high-end frequency inverter will be presented.

2013-09-12 – Mitsubishi Electric launches new webstore for automation software

The new e-F@ctory Alliance software webstore is a first for the automation business and offers a huge range of incredibly useful ‘approved’ automation software and dedicated function blocks available for instant download. Programs on offer also include partner solutions that have been developed alongside Mitsubishi Electric to support users to find best practice solutions for their automation...

2013-05-29 – Mitsubishi Electric programming software and Simple Motion Modules certified compliant with PLCopen standard

Mitsubishi Electric Europe has been awarded a Certificate of Compliance for Function Blocks for Motion Control by PLCopen for its Simple Motion Module and GX Works2 software. The certification recognises the compliance of these products with IEC61131-3 standards in implementation of motion control function blocks, and demonstrates Mitsubishi Electric’s commitment to best practice in automation...

2013-06-04 – e-F@ctory Alliance exhibition launches into the virtual world

The e-F@ctory Alliance* trade show is the first full exhibition to be staged using Mitsubishi Electric’s new virtual exhibition platform, and the first major virtual show to deliver a convincing and rewarding visitor experience.

2013-04-24 – Mitsubishi Electric and Raima create secure data handling process

Controlling and managing a complex system is difficult at any time. However, users in the process (ex. water, petro-chemical) and infrastructure industries such as surface rail, airports or underground metro systems have the added complexities of having to do the same over extreme distances with the possibility of 1000's of I/O points.

2013-04-15 – Energy Efficiency with Mitsubishi Electric and KH-Automation at WASSER BERLIN 2013

At the WASSER BERLIN INTERNATIONAL Show from 23 – 26 April 2013, Mitsubishi Electric and KH-Automation Projects will present automation solutions for the water sector. The two companies specialise in systems for the water, waste water and waste materials sectors. The focal points are energy efficiency, remote maintenance, preventative maintenance and condition monitoring.

2013-03-05 – Smart conveyor lines up quiches for precision baking

In the drive to reduce packaging and its resultant waste, a specialist machinery builder has developed a pressureless queuing conveyor for collating quiches prior to baking.

2013-02-13 – Mitsubishi Electric optimises Irish waste water treatment and purification plants in record time

The aim of the operators of a waste water treatment plant and four associated purification plants in the East of Ireland was to reduce ongoing operating costs through modernisation. In order to do that, the plant was brought right up-to-date by installing Mitsubishi Electric automation components. This involved taking particularly diverse performance requirements into account as well as ...

2013-02-12 – The Production-integrated Enterprise in 2020

Globalisation, increasing customer sophistication and resource scarcity are all challenges facing the process industries, and by 2020 these will be even more acute. Meeting these challenges will depend on structures that will enable wholly automated planning, dynamic scheduling and fully optimised production processes to control unit production cost.

2011-09-14 – Mitsubishi Electric supports Weihenstephan Standards

The FX, System Q and C Controller product ranges from Mitsubishi Electric now all support the Weihenstephan data acquisition and communication standards.

2011-08-30 – Mitsubishi Electric EPLAN data is now available on the EPLAN data portal

EPLAN users can now import electrical wiring data for Mitsubishi Electric modular PLCs and servo/motion products into their CAE (Computer-aided engineering) projects directly from the EPLAN Data Portal.

*Note: The texts and illustrations are copyright protected by Mitsubishi Electric. They may be freely used provided they are used exclusively for reporting and informing about Mitsubishi Electric or our products. The use of these texts and illustrations beyond press or radio reporting purposes requires our explicit consent.

Inquiries
Contact
Knowledge Base
Help