Start main contents

  • Register
  • Login

Factory Automation

Print page

Factory Automation

Hannovermesse

What we will show

From 23.-27.April 2018 Mitsubishi Electric will demonstrate at the Hanover Fair Industry 4.0 solutions, developed in the context of our own e-F@ctory concept.

360° digitization, that means we will present trend topics like digitization, edge computing etc., but also OEE, predictive maintenance and monitoring/analysis tools for drive, control and robotics, energy management as well as collaborative and cooperative robots.

Digital transformation in its smart way

At our booth you will learn how digitization can make your production more flexible. The intelligent use of integrated automation platforms opens up new potential for production optimization.

Among other things, all applicative data from the robotics, drive and control systems of the Mitsubishi Electric automation world as well as the partner applications will be transferred to the superordinate SCADA system MAPS (Mitsubishi Androit Process Suite).

Experience live how data from the production environment is captured and transmitted to MAPS for visualization, monitoring, and process analysis, and how Mitsubishi Electric's e-F@ctory concept provides a way to deliver cyber-secure, open edge computing solutions for direct production connectivity to develop the cloud.

Solution Sessions von Mitsubishi Electric auf der Hannover Messe 2018

Poka Yoke – Guided Operator Solutions

The art of a perfect manual assembly work place. In cooperation with our premium system partner Handke Industrie-Technik GmbH we present a complete solution that can be used to make manual assembly applications error-free.

In addition to the flexibility in the creation of manual assembly work place from Handke, the Poka Yoke Controller offers many more options. The system offers a wide variety of sensors, enables the use of electrical industrial screwdrivers and / or barcode scanners and can be expanded as well as integrated into existing production processes.

As a special feature, Mitsubishi Electric accesses the full shelf of its own portfolio and introduces a robot with the safe protective skin MELFA SafeSkin at the manual workstation. The standard MELFA robot can thus cooperate directly with humans and support the manual assembly work place.

Discuss with us and convince yourself on site of the combination of core competencies - the assembly technology as well as Japanese Lean approach to the prevention of errors within the production.

More information about Guided Operator Solutions

Collaborative robot

While the precision of some collaborative robots may be reduced in comparison with industrial versions, the Mitsubishi Electric model’s performance characteristics mirror those of the company’s industrial autonomous robot range. This means a repeat accuracy of ±0.02 mm, despite the inclusion of sensitive force/torque sensors. Load capacity of the shown robot model is between 5 and 6 kg and reach is between 800 and 1000 mm.

As well as performance, Mitsubishi Electric has also addressed ease of use, with innovative and, to date, unique control and programming options. A touch-screen operator terminal, which can be plugged into the robot, provides an intuitive interface to ‘teach’ the robot its task, without any special programming expertise. The teach functionality includes a ‘direct control’ mode which allows the operator to move the robot from position to position, by hand and with controlled force. Once the set-up is complete, the operator terminal is easily removed to give the robot full freedom of movement.

See the prototype live at our booth

Always the right answer - Servo Open Network

Whatever you are looking for, with the flexible serviceability of servos with open network connections you already have the right answer to the challenges of tomorrow.

Your advantage: Whether EtherCAT, Profinet, CC-Link IE Field or Ethernet / IP - you now have a compatible and powerful drive solution at hand for all systems.

We'll give you the freedom: choose the MELSERVO MR-J4 series now and meet the changing international performance requirements of today's high-end motion / control machines in a single solution.

Finden Sie Ihr passendes Netzwerk hier

Technology with foresight: our solutions for smart condition monitoring - predictive maintenance

Mitsubishi Electric offers the opportunity with its ready-made Smart Condition Monitoring Kits as a powerful complete solution for easy integration into existing applications. Compared to conventional monitoring concepts, the modular Plug & Play system not only analyzes classic machine data such as temperature, but also vibration-dependent parameters.

Typical application areas for the kits are pumps, compressors, fans, conveyor belts, but also processing systems from different industries.

For this we present you on the stand 2 different SCM kits

-SCM Kit DRIVES for the lower power range with the integration of up to 2 sensors
-SCM Kit COMPACT for up to 6 sensors

Let our experts advise you!

Zur unseren Informationen zum Thema Smart Condition Monitoring – Vorausschauenden Wartung

The e-F@ctory concept in the context of Industry 4.0

'Industry 4.0' is nowadays an important keyword. The developments are progressing and in times of I4.0 and IIoT no company can’t afford to focus on this important topic. Mitsubishi Electric has been involved in digitization since 2003. With the e-F@ctory concept, we support our clients in the advancement of their entrepreneurial projects in the field of industrial automation and information technology in the context of the increasing digital transformation.

Let us advise you on how we can support you in your digitization process.

Erfahren Sie hier mehr über unser e-F@ctory Konzept

Finally

At the Mitsubishi Electric booth further technical innovations will be presented to highlight the demand for various production-side applications, along with industry-specific solutions for a variety of business sectors. All exhibits are designed to increase efficiency and reduce costs while providing answers to specific challenges such as traceability, quality, safety and sustainability.

Your way to us

You will find us in hall 17 booth D40


The fields marked by a * are mandatory.

Your way to Hannovermesse

Please enter the text you can see on the picture in the field below. If you can not read the picture please click "Refresh".

Sicherheitscode Refresh

Back

Page top